Why Custom-Made? Because It’s Timeless

Back to Top

Closeup of S&C Custom Metal-Enclosed Switchgear. There are 10 bays, each with a heavy-duty metal door closed over it. Each door has a metal padlock door on it. The entire switchgear lineup is light gray and there is a green S&C logo on one of the doors.

It sounds like a riddle, but it’s not meant to be one:

What remains timeless even as fashions change?

Answer: customization.

That’s why we at S&C are so proud of our Custom Metal-Enclosed Switchgear (MES). For more than a century, we’ve been partnering with customers to design switchgear solutions that are tailored from the ground up.

Each solution is a reflection of collaboration—your needs, your goals, our expertise—brought together in one custom-engineered system. The result: exceptional reliability and significant cost savings.

Our Custom MES is what we say it is: custom.
profile picture

Why Customization Is Timeless

Here’s another kind-of-a-riddle question:

What’s one thing people have loved since the beginning of commerce?

Answer: saving money.

When compared with conventional switchgear options, S&C’s Custom MES saves you money in two ways:

  1. Upfront cost: An equivalent lineup of conventional metal-clad switchgear costs more than Custom MES.
  2. Lifetime cost: While breaker-based gear can require intensive regular maintenance, Custom MES requires significantly less. Plus, the high-quality components in Custom MES require less maintenance over the lifetime of the gear than either metal-clad gear or pre-engineered MES.

That means fewer interruptions, lower total costs, and more peace of mind—benefits our customers have valued for generations.

When We Say ‘Custom,’ We Mean It

No riddles or questions here—just a straightforward statement:

Our Custom MES is what we say it is: custom.

At S&C, our blueprint starts with you. Every solution we build starts with a conversation, not a catalog.

We roll up our sleeves alongside you to understand your system, your challenges, and your vision. Then, together, we create the switchgear that precisely fits your needs.

Want to see customization in action? Watch this video:


Interested in learning more? Contact us to talk about your project and how S&C’s Custom MES can meet your specific needs.

CONTACT US

专家

Joseph Matamoros

出版日期

十月 27, 2025