S&C Named Winner of Chicago Innovation Awards Competition for TripSaver Dropout Recloser

Bookmark and Share

S&C Electric Company was named one of ten winners in this year’s Chicago Innovation Awards Competition, for their unique new TripSaver™ Dropout Recloser. The winners — chosen from 249 nominees from four states — were judged on their success in satisfying unmet needs in the marketplace. They were honored at a ceremony held at the Goodman Theatre in downtown Chicago on October 22nd.

TripSaver protects overhead lateral circuits on electrical distribution systems. Used in lieu of a more commonly applied fuse cutout, it improves system reliability by eliminating the permanent outage which results when the cutout responds to a temporary fault. Offered in system voltage class ratings of 15.5 and 27 kV, this self-powered, electronically controlled vacuum recloser can be installed in new or existing cutout mountings. A two-insulator branch-feeder style mounting is also available. TripSaver requires no programming or batteries.

About the Chicago Innovation Awards

Kuczmarski & Associates and the Chicago Sun-Times established the Chicago Innovation Awards in 2002 as an annual program to honor significant innovations introduced by Chicago-area companies. Each year they honor 10 winners who have introduced products or services that uniquely fill unmet needs, generate a competitive response in the marketplace, exceed market expectations, and achieve financial success. For more information and to see all the winners, visit www.ChicagoInnovationAwards.com.

This entry was posted in Overhead Distribution and tagged . Bookmark the permalink.

Comments are closed.