S&C Solution Protects Critical NASA Facility From Power Outages

Bookmark and Share

S&C Electric Company, a global smart grid leader, today announces that it has delivered, installed and commissioned a PureWave® UPS Uninterruptible Power Supply for NASA’s Goldstone Deep Space Communication Complex managed by Jet Propulsion Laboratory in Pasadena, California. S&C’s PureWave UPS provides the highest level of protection against outages available today. In the event of a power disturbance, it transfers electrical load to the back-up system in a fraction of a second.

NASA’s Goldstone Communication Complex, which handles critical deep space spacecraft transmissions, includes sensitive equipment that can be disrupted by the briefest of power outages. The facility typically has run on back-up diesel generators during critical spacecraft transmissions to ensure electric service reliability. However, a recently enacted California state law imposed new restrictions on generator emissions, which led NASA to seek a battery-based UPS solution.

The PureWave UPS allows NASA to provide back-up power for the tracking facility in a greatly simplified and reliable manner. The UPS system has already protected the facility against voltage dips and utility outages while also allowing compiance with the California state air pollution law.

The PureWave UPS supports the entire 3.8 megawatt load with clean power for up to 60 seconds, eliminating all of the short term  utility based power quality problems. It supports reduced loads for up to 180 seconds, and in the rare event of an extended outage, the unit seamlessly transfers the facility load to the back-up generators.

“The need for higher power quality and reliability is growing, and S&C’s PureWave UPS is a field-proven solution that is protecting critical facilities worldwide, including data centers and highly sensitive government facilities,” says Jim Sember, S&C Vice President—Power Quality Products. “The PureWave UPS provides an effective power quality solution for facilities where even very brief power disturbances can have significant consequences.”

This entry was posted in Power Quality and tagged . Bookmark the permalink.

Comments are closed.