About S&C Electric Company
Our Commitment to Quality
Quality design and flawless manufacturing have been central to S&C’s philosophy throughout its 90-year history. Reliability and durability are engineered into every S&C product. Rigorous procedures ensure accurate manufacturing and delivery to the customer.
Certification
Because of its quality initiatives, S&C is known in its industry as the leader in long-term value. S&C–US received certification to the ISO 9000 standard in 1998. Presently all central operations, the Fuse Products Division, the Switch Products Division, the Polymer Products Division, and Power Systems Services are certified to ISO 9001:2000.
The S&C–Toronto subsidiary was certified to ISO 9001 in 1995 and presently is certified to ISO 9001: 2000. S&C’s regional center in Brazil received certification under the ISO 9001 in May 2001. The regional center in China received ISO 9001 certification in 2002. Presently, both regional centers are certified to ISO 9001: 2000.
All of S&C’s operations include recognized quality procedures and use feedback mechanisms that identify potential problems so they can be addressed.